Solid Edge Design Intent Parameters Not Retained Between Solid Edge Sessions

2024-06-05T05:40:33Z
PART/SHEETMETAL

Summary


Details

When using Synchronous Technology in Solid Edge, the design intent parameters are not retained between sessions. Specifically, if a specific parameter is deactivated in one session, it will be reactivated by default in the next session.

Solution

This behavior is by design in Solid Edge. The Design Intent parameters are always reset to default settings upon restarting Solid Edge. This ensures consistent behavior for all sessions.

Currently, there is no method to modify these default conditions. 

This is documented in the Solid Edge Help documentation, which can be accessed here:

Using the Advanced Design Intent panel - https://docs.sw.siemens.com/en-US/doc/246738425/PL20220830878154140.design/relateman1d


KB Article ID# PL8794481

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES