Exporting 3DS Max Files to Solid Edge

2024-06-04T22:13:26Z

Summary


Details

Users need to export files from 3DS Max and import them into Solid Edge. A user attempted to use an STL file format but encountered an issue where the file would not open in Solid Edge.

Solution

To successfully export a file from 3DS Max and import it into Solid Edge, use either the ACIS (.sat) or IGES (.igs) file formats. These formats are supported by both 3DS Max and Solid Edge and should facilitate a smooth transfer between the programs.

1. Export from 3DS Max:

  • Open your model in 3DS Max.
    • Go to the "File" menu and select "Export."
      • Choose either "ACIS (.sat)" or "IGES (.igs)" as the file type.
        • Save the file to your desired location.

          2. Import into Solid Edge:

          • Open Solid Edge.
            • Go to the "File" menu and select "Open."
              • Browse to the location of the exported file.

                Select the ACIS (.sat) or IGES (.igs) file and open it.

                Using these steps, you should be able to transfer your 3DS Max models into Solid Edge without compatibility issues.

                KB Article ID# PL8794454

                Contents

                SummaryDetails

                Associated Components