The "Retrieve from Teamcenter" command becomes unavailable in ATTI

2024-07-02T13:45:16Z

Summary


Details

Sometimes after the "Find All Linked Documents" command is used in Add to Teamcenter Interactive the "Retrieve Data from Teamcenter" command becomes inactive. There is no indication in ATTI of what the problem is.

Platforms
  • all n/a-n/a
Release Versions
  • Solid Edge V224.0
Solution

The "Retrieve Data from Teamcenter" command will become inactive if there are any issues found with the unmanaged data loaded into Add to Teamcenter Interactive, such as broken links or files in the select set that have the file status set to "Released". Go to View -> Expand All then scroll down the list of files to see which files have issues and what the issues are.

Notes

KB Article ID# PL8794417

Contents

SummaryDetails

Associated Components