Solid Edge Unable to Use PMI Centerline Command in Solid Edge

2024-06-04T13:20:19Z
APPLICATION

Summary


Details

Users encounter a warning message stating, "You do not have a valid license to use this command," when attempting to use the PMI Centerline command in Solid Edge Premium

The error suggests contacting a Solid Edge reseller or technical support for resolution.


Solution

The issue arises because the PMI Centerline command falls under enhanced Product and Manufacturing Information (PMI) functionality, which is not included in the standard Solid Edge Premium license. Enhanced PMI features, including Centerline, require additional licensing through the Model Based Definition (MBD) add-on product.

KB Article ID# PL8794376

Contents

SummaryDetails

Associated Components

APPLICATION: MBD