Displaying Dimensions as Numbers in Solid Edge

2024-06-04T11:54:07Z

Summary


Details

Dimensions are shown as text labels (e.g., "DimA, DimB") instead of numerical values (e.g., "600mm, 20mm") in Solid Edge models.


Solution

This issue occurs when the "Show All Names" command is enabled. To display dimensions as numerical values, follow these steps:

  1. Open the model in Solid Edge.
    1. Expand the Pathfinder pane.
      1. Navigate to PMI (Product and Manufacturing Information) -> Dimension tree.
        1. Right-click on any PMI dimension.
          1. Select "Show All Values" from the context menu.

            This action will change the display from text labels to numerical values. For more information on related commands, refer to the following Solid Edge help topics:

            "Show All Formulas Command" - https://docs.sw.siemens.com/en-US/doc/246738425/PL20220830878154140.design/shwformulas1c

            "Show All Names Command" - https://docs.sw.siemens.com/en-US/doc/246738425/PL20220830878154140.design/shwnames1c

            "Show All Values Command" - https://docs.sw.siemens.com/en-US/doc/246738425/PL20220830878154140.design/shwvalues1c

            KB Article ID# PL8794353

            Contents

            SummaryDetails

            Associated Components