Teamcenter Structure does not matches with NX Assembly Structure

2024-06-30T16:19:44Z

Summary


Details

Teamcenter Structure does not match with NX Assembly Structure

While creating NX Assemblies sometimes users tend to swap the sequence of the Parts/Subassemblies in NX, but after doing so, when they save the data in NX and go back to Teamcenter, the swapping of the components is not reflected in the Teamcenter Structure Manager.

The sequence of the Assembly Components does not match with the NX Assembly Structure.

Solution

The order in the Teamcenter Structure manager is controlled using the "Find No" column.

NX stores the order based on its last saved state.

you can control the order by modifying the Find No column in the TC Structure Manager application.

NX has the Chronological order of creation but TC does not support the same for now, it always works based on Find No or based on the Column selected for ordering.

Notes

KB Article ID# PL8794322

Contents

SummaryDetails

Associated Components