Solid Edge How to Ensure Base Reference Planes are Always On When Opening a Part File

2024-06-04T05:26:01Z
PART/SHEETMETAL

Summary


Details

Users need a way to ensure that base reference planes are always turned on by default when opening a new part file. The current process requires users to manually turn on the base reference planes each time a new part file is opened, which can be time-consuming.

Solution

To have the base reference planes always turned on by default when creating a new part file, modify the part template file by following these steps:

  1. Open the part template file.
    1. Turn on the base reference planes.
      1. Save the modified template file.

        By using the modified template file, the base reference planes will automatically be turned on for new part files created with this template.

        KB Article ID# PL8794249

        Contents

        SummaryDetails

        Associated Components

        PART/SHEETMETAL: OTHER