Importing and Editing PDF Files in Solid Edge

2024-06-04T05:10:54Z

Summary


Details

Customer uses Nemetschek Allplan to import and edit PDF files. This process includes capturing points from lines and constructing 2D models based on the imported PDF files. The company is aware that similar functionalities are available in competitor CAD products. They desire the same capability in Solid Edge, specifically the ability to import PDF documents saved with CAD systems and further process the original geometry.

Solution

Existing Enhancement Request (ER):

There is an existing enhancement request (ER) in place for adding the functionality to import and edit PDF files in Solid Edge. This request aims to allow users to capture points from lines within the PDF and use this data to build 2D models.

Current Capabilities:

As of now, Solid Edge does not natively support the direct import and editable use of PDF files in the manner described. Users seeking this functionality are encouraged to use alternative workflows, such as converting PDFs to a supported file format using third-party tools before importing them into Solid Edge.

Future Updates:

The development team is aware of the demand for this feature and is considering it for future updates. Users can monitor the release notes of upcoming Solid Edge versions for any updates regarding this feature.

For the latest information on supported file formats and upcoming features, users should refer to the official Solid Edge documentation and support resources.

KB Article ID# PL8794243

Contents

SummaryDetails

Associated Components