Optimizing Page File Size for Solid Edge Performance

2024-06-03T10:02:42Z

Summary


Details

A user reported concerns about the recommended page file size for Solid Edge. The readme file suggests setting a custom page file size to double the RAM size for optimal performance. The user, who is upgrading to new hardware with 64GB RAM and a 512GB SSD, questioned the relevance of this requirement, noting it would occupy a significant portion of their disk space.

Solution

The requirement to set a page file size to double the RAM is still relevant and is not based on outdated technology. The page file serves as a backup for system memory, ensuring stable operation when RAM is fully utilized. Modern operating systems, like Windows 10 and 11, may require a page file size up to 4 times the RAM.

For Solid Edge, it is recommended to set the page file size to 2 times the RAM for both the initial and maximum sizes. This practice prevents the need for the page file to auto-grow, which can be slow and cause application crashes. In scenarios involving large assemblies and drawings, users may need to increase the page file size beyond 2 times the RAM to ensure stability and prevent crashes.

For further information, refer to the Microsoft resource: Introduction to Page Files.

KB Article ID# PL8794128

Contents

SummaryDetails

Associated Components