Arc and spline shapes are not exported smoothly in 3D PDF

2024-06-04T02:48:14Z

Summary


Details

When arcs and splines are exported as 3D PDF and viewed those objects in Acrobat Reader, they don't appear as smooth curves.

Reproduced Steps:

1. Create arcs and splines (by Sketch or etc.)


2. PMI tab > Publish > Technical Data Package tab > Templates > Method > 3D PDF > select any template listed in template selection window > OK

3. Open the PDF in Acrobat Reader


Solution

This behavior is due to a problem that occurred in NX 2212 and lower, and has been fixed in NX 2312.

Workaround : No


Notes

The edges that make up solid or surface shapes are smooth, but this is an issue that only occurs with sketches and other wireframe shapes.


**Please refer to PL8794050 for Japanese article.

Release Versions
  • NX V1980
  • NX - TECH_DATA_PKG V1980
Platforms
  • Windows x64 11
  • Windows x64 10

KB Article ID# PL8794052

Contents

SummaryDetails

Associated Components