Not going to MBD Query tab

2024-06-04T02:46:47Z

Summary


Details

When running "Find all PMI" from Reuse Library navigator, control is transferred to MBD Query navigator and the results are displayed. When running "Find all PMI" again from Reuse Library Navigator, it does not transfer to MBD Query Navigator.

Reproduced Steps:

1. Prepare a model and PMI dimension

2. Reuse Library Navigator > Folder View window > MBD Query Logical Rules > General Member Select General window > Find all PMI


3. Control automatically transfers to the MBD Query navigator, where the results are displayed.


4. Again, perform step 2 above

** not move to "MBD Query" navigator.


Solution

This behavior is due to NX problem that has been occurring since NX 2212 and is fixed in NX 2412 Series.

Workaround: The command is executed successfully, so please explicitly move to MBD Query navigator.


Notes

The problem occurs with all commands, not just "Find all PMI".

**Please refer to PL8793908 for Japanese article.

Release Versions
  • NX V2312
  • NX - MBD V2312
Platforms
  • Windows x64 11
  • Windows x64 10

KB Article ID# PL8793909

Contents

SummaryDetails

Associated Components