Controlling the display of scene dialogs and command dialog

2024-06-10T22:11:33Z

Summary


Details

When inserting or editing features, the scene dialog and command dialog may overlap with the model, making it difficult to use. Is it possible to hide the scene dialog and command dialog?

Reproduced Steps:

1. Creating or editing a feature such as Edge Blend



Solution

By F3 key while a command is running, you can hide the scene dialog without terminating the command.


In addition, by F3 key repeatedly, you can hide the command dialog and show all of it.


Notes

Using scene dialogs in Modeling

https://docs.sw.siemens.com/en-US/doc/209349590/PL20230425446868577.modeling/param_opts_dyn_input_boxes

**Please refer to PL8793901 for Japanese article.

Release Versions
  • NX V11.0.2
  • NX V12.0.2
  • NX V1847
  • NX V1872
  • NX V1899
  • NX V1926
  • NX V1980
  • NX V2007
  • NX V2206
  • NX V2212
  • NX V2306
  • NX V2312
Platforms
  • Windows x64 11
  • Windows x64 10

KB Article ID# PL8793902

Contents

SummaryDetails

Associated Components