The customer reported an issue where new fonts installed in the draft environment are not displaying correctly when converting the draft into a PDF file. The customer provided an example draft and the fonts for reference.
SolutionUpon investigation, it was determined that the issue is caused by a Restricted License on the provided fonts.
Solid Edge does not allow the embedding of fonts with a Restricted License into PDF files. It is important to note that using a different software, such as Word, to embed the fonts into a PDF file would be a violation of the licensing agreement for the font.
To resolve this issue, the customer has two options. They can either find a font with a less restrictive licensing type or they can contact the author of the font to request a change in the license restriction.
For more information on font licensing and the different types of font embedding, please refer to the following third-party link:
https://www.high-logic.com/fontcreator/manual15/fontproperties-font.html
Where the following useful information regarding font embedding rights is provided: