Solid Edge What are the Three Options for 'Copy to Working Folder'?

2024-07-02T11:46:55Z
APPLICATION

Summary


Details

In the Solid Edge Standard Parts - Parts Management Administrator are three different settings for the 'Copy to working folder' option.  The option can be unchecked or checked as usual but there is also a black little square.  What does that mean?


Solution
Off - The option is off for all users and users cannot change that in PartFinder

On with a simple checkmark - The option is on for all users and users cannot change that in PartFinder

On with a black little square - The option is available for users and can be set in PartFinder

Notes

1. PartFinder is the user interface inside Solid Edge assembly that allows user to place a Standard Part.

2. For further information about Standard Parts see Solid Edge Standard Parts FAQ collection

3. For further information about working folder see Solid Edge Standard Parts working folder

KB Article ID# PL8793780

Contents

SummaryDetails

Associated Components

APPLICATION: STANDARD_PARTS