Editing sketch sections of Variational Sweep

2024-09-16T12:05:26Z

Summary


Details

Editing sketch sections of Variational Sweep.

Solution

Please see the NX video above and refer to the following steps below.

The sketch section dimensions must be converted to expressions for them to appear in each section of the Variational Sweep.  The Add/Remove Expression must be toggled on for each dimension which can be completed using the steps below.   

1.  Right mouse button click on the Variational Sweep feature and select Edit with Rollback.

2.  Click on Sketch Section in the dialog as seen below.


3.  Right mouse button click on each dimension and select Add/Remove Expression from the drop-down menu.  Click Finish in the sketch once all dimensions have been changed.

Note - the selection filter can be set to 'Dimension' in order to select multiple dimensions to complete this in a single operation.

4.  Now the sections of the Variational Sweep can be selected in the dialog, and the dimensions in the graphics screen can be selected to modify.


Notes

KB Article ID# PL8793133

Contents

SummaryDetails

Associated Components