Can a part from a Functional Release of NX be opened in a Monthly Update release.

2024-05-23T18:17:39Z

Summary


Details

With the new 'NX Series' continuous releases, can a part from new Functional Release NX2306 be opened in the Monthly Update (MU) release of NX2212?

Solution

No, the NX2306 part cannot be opened in NX2212 or any of the Monthly updates, it will raise the error "Part is from a newer version of NX than this one".

The Functional Releases will have a newer Parasolid version that are not backward compatible. The part can be opened between the Monthly Updates for the NX release that the part was created in, and in newer NX Releases.

KB Article ID# PL8792716

Contents

SummaryDetails

Associated Components