Quick Pick menu does not open.

2024-05-23T18:17:20Z

Summary


Details

After selecting the Quick Pick icon, the quick pick menu that list the objects does not open.

Solution

If Reset Dialog Memory does not fix the problem, change the Display Resolution so that if the Quick Pick menu is outside the window area it will bring into the window and display. The User can then move the dialog closer to the selected objects, then change the display resolution back to the original settings.

KB Article ID# PL8792705

Contents

SummaryDetails

Associated Components