NX start offset 3 out of range for UString::substr error when starting NX

2024-05-22T13:09:10Z
NX for Design

Summary


Details

start offset 3 out of range for UString::substr error when starting NX

Platforms
  • na windows-1064
Release Versions
  • NX V2312.3000
Solution

It was identified that the source of the issue was a corrupted site level customer default file.

The customer defaults file was simply copied from the old NX version so it was removed. Then started NX normally and then imported the old file through the customer defaults user interface.

Notes

KB Article ID# PL8792642

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX