Saving a Flattened Sheetmetal Part as STEP

2024-05-29T13:57:03Z

Summary


Details

In this example, the user wants to quickly save a flattened Sheetmetal part as a STEP file.

However, "Save as Flat" will not provide STEP as an option for exporting.

Solution

 There is a quick way to get the flattened model saved:

1) Switch to "Flatten" Environment - quickly done by double-clicking on "Flat Pattern" in PathFinder

2) Now do a "Save as Translated".  This will offer the option of STEP as a format for exporting.  The command will take current, active model - which is flattened - and export it.

KB Article ID# PL8792615

Contents

SummaryDetails

Associated Components