Advanced PMI functionality not available

2024-05-19T06:52:57Z

Summary


Details

The customer reported that the "Advanced PMI" function was not being activated in Solid Edge, despite having a valid license for it. The customer provided screenshots  showing that the license file was present and that the command was not enabled.



Solution

After reviewing the provided information, it was determined that the issue was related to the license activation process. The customer had not checked out the Advanced PMI license, which was causing the functionality to remain disabled. The following steps resolve the issue:

1. In Solid Edge, locate the "Solid Edge PMI License" icon/button.


2. Click on the "Solid Edge PMI License" button to activate it.

3. After activation, the "Solid Edge PMI License" icon will be greyed out, indicating that the Advanced PMI functionality is now enabled.


4. Test the Advanced PMI command to verify that it is working as expected.


KB Article ID# PL8792113

Contents

SummaryDetails

Associated Components