Solid Edge Want to download shared files on a Teamcenter Share project.

2024-05-20T15:16:20Z
PART/SHEETMETAL SETUP

Summary


Details

Not able to download files from shared project in Teamcenter Share.

Platforms
  • INTEL windows-1064
Release Versions
  • Solid Edge V224.0
Solution

When the person shares the project. they must choose to share using the option "Review + Download" or "Full access" in order to have download privileges.

Notes

KB Article ID# PL8792013

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES