How to adjust the toe joint in Process Simulate Human?

2024-05-16T12:12:04Z

Summary


Details

How to adjust the toe joint in Process Simulate Human?

While performing Human Simulation there are some rare occasions when human toe joint is also required to be adjusted and tested for the specific task.

In Classic Jack 9.0 we were able to adjust toe joint, but the same or corresponding feature could not be found in Process Simulate.

So, the question is how to adjust toe joint in Process Simulate Human?

Solution

This is possible, but not through the Human Posturing User Interface which can be seen in the Process Simulate's Human menu.

Actually, some of the lesser used joints are not exposed here.

Additional human commands which are not found in the Human tab of the ribbon can be added via the Customize the ribbon command.

Once the command is added in the ribbon , you can select the human and execute the command.

From the drop down list of Joint Jog window, select the required feet and now you can adjust or jog the toes of human.

Hope this helps.

KB Article ID# PL8791922

Contents

SummaryDetails

Associated Components