Options file "vendor.opt" not being used by FlexNet licensing

2024-05-20T12:12:57Z

Summary


Details

The customer has implemented the "vendor.opt" file, but it is not read by the license manager.

How to make the Siemens License Server (SLS/SALT) make use of the options file?

Platforms
  • na windows-1064
Release Versions
  • Solid Edge V224UPD5
Solution

This is what is needed:

-place the options file in the FlexNet install folder, "C:\Program Files\Siemens\License Server".-add the name of the options file in the used license file, after the vendor daemon name.

[If placed in another location include the full search path]


-restart the License server

Now the Licens server picks up the options file, as seen in the "saltd.log".


Notes

KB Article ID# PL8791789

Contents

SummaryDetails

Associated Components