Version compatibility between NX and Solid Edge

2024-05-17T02:43:07Z

Summary


Details

When opening Solid Edge data in NX, I think the supported Solid Edge versions differ depending on NX Series. Are there any documents that contain this information?

Solution

From the link below, Solid Edge and NX version compatibility(Solid Edge 2024 and NX 2306)information can be confirmed.

https://docs.sw.siemens.com/en-US/doc/246738425/PL20220830878154140.importing_exporting_files/ugse1a

Notes

For updated information, please check the documentation of the new version that will be released in the future.(Example : Solid Edge 2024 and NX 2306)

“Solid Edge” > “Documentation” > “Solid Edge 2024 (2310)” > “Importing and exporting files with Solid Edge” > “Working with NX files in Solid Edge” > “Solid Edge and NX version compatibility”

*** At ”Solid Edge” > “Documentation” site, you can search for it under “Importing and exporting files".

**Please refer to PL8790568 for Japanese article.

Release Versions
  • NX V2312
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8790569

Contents

SummaryDetails

Associated Components