Tecnomatix Oracle CPU for April 2024 is Available

2024-05-07T10:47:44Z
eM-Server

Summary


Details

Oracle has released a quarterly Critical Patch Update to fix vulnerabilities in Oracle database products: Oracle Critical Patch Update for April 2024.

These patches are available for download by licensed customers at https://support.sw.siemens.com

Go to Support Center and choose the Oracle Product. Click on Downloads, then choose from the 'Select a Version' drop down.To access the latest Opatch installers, choose the Version and Opatch from the 'Select a Version' drop down.

The patches include:

Oracle 19c (19.23.0.0.240416)

p36233263_190000_Linux-x86-64.zip

p36219938_190000_MSWIN-x86-64.zip

Oracle 19c Opatch (12.2.0.1.42)

p6880880_190000_Linux-x86-64.zip

p6880880_190000_MSWIN-x86-64.zip

Teamcenter supports these versions of Oracle Database:

For the latest information, please refer to the Teamcenter Platform Matrix

at Support Center. It is located under Support White Papers under Teamcenter

Download.

Oracle 12c - Teamcenter 10.1.5, Teamcenter 11.x, Teamcenter 12.x

Oracle 18c - Teamcenter 11.x, Teamcenter 12.x

Oracle 19c - Teamcenter 12.4.x, Teamcenter 13.x, Teamcenter 14.x

KB Article ID# PL8790186

Contents

SummaryDetails

Associated Components

Oracle Database