After importing third-party files into Solid Edge, users notice a blue circle "i" symbol on the imported features. The purpose and significance of this symbol are unclear.
The blue circle with an "i" symbol indicates that the imported geometry has not been optimized. To ensure optimal performance and quality, it is recommended to follow best practices when working with imported CAD data in Solid Edge.
Effects of Non-Optimized Geometry:
Non-optimized geometry can lead to several issues, including:
Window Display Performance:
Modeling Problems:
Draft Drawing View Creation or Updates:
Optimize Command:
Solid Edge provides the Optimize command to address these issues and improve the precision and quality of imported models. The Optimize command performs the following tasks:
Best Practices for Working with Imported CAD Data:
To ensure a smooth workflow and optimize the quality of imported CAD data, it is recommended to follow these best practices:
Note: Siemens DI SW will not address any issues encountered when working with imported unoptimized CAD data. Therefore, it is crucial to run the Optimize command to ensure optimal performance and avoid potential problems.
Conclusion:
Working with imported CAD data in Solid Edge requires optimizing the geometry using the Optimize command. By following best practices, such as running the Optimize command and regularly updating imported models, users can enhance precision, improve performance, and avoid potential issues associated with non-optimized geometry.
NotesFor more Solid Edge STEP related articles, please refer to the "Solid Edge STEP FAQs Collection"
Utility for Automatic Optimization of Imported CAD Models in Solid Edge
Solid Edge 2024 Help documentation on "Working with non-CAD data".
Solid Edge 2024 Help documentation on "Optimize command".
Solid Edge 2024 Help documentation on "Using Geometry Inspector".
Solid Edge 2024 Help documentation on "Geometry Inspector command".