New Study template default values missing

2024-08-26T15:40:05Z

Summary


Details

In PS standalone, when using the "Create New Study" option on the welcome splash screen, the Default values for the New Study "Template" and "Study Type" do not auto populate. These are the expected and missing values:

Template: "C:\Program Files\Tecnomatix_2301.0\eMPower\Templates\DefaultStudy.pszt"

Study: "RobcadStudy".Without them, a study cannot be created.

Platforms
  • all n/a-n/a
Release Versions
  • Tecnomatix V2301
Solution

Add or modify the registry ahead to get the value populated (sample install path shown as value). 

Key:

HKEY_CURRENT_USER\Software\Tecnomatix\TUNE\NewAssembler\Commands Info\EngineeringDataOperations\Dialogs\CUiEDONewStudyForm \Template File Path

Value:

C:\Program Files\Tecnomatix_2301.0\eMPower\Templates\DefaultStudy.pszt

Notes

KB Article ID# PL8790139

Contents

SummaryDetails

Associated Components