Parameters entered in the IGES export dialog are not saved in dialog memory

2024-05-17T02:42:08Z

Summary


Details

The command was performed after changing the initial values of "SP-Curve/B-Surface Tolerance" and "Maximum Line Thickness". If checking the IGES dialog again, it returned to the initial value before the change.

Reproduced Steps:

1. File > Export > IGES > Advanced tab > Parameters


2. After change two parameter values, click OK to finish the command

- SP-curve/B-surface Tolerance=0.01

- Maximum Line Thickness=1.0


3. Performing IGES Export again and confirm the parameters


Solution

This behavior is due to NX problem and is going to fix in NX 2406.

Workaround : There is no WA, so please input the parameters each time.

Notes

There is no effect when the command is executed, and it's correctly output by the input parameter values.

**Please refer to PL8789979 for Japanese article.

Release Versions
  • NX V2306
  • NX - TRANSLATOR V2306
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8789981

Contents

SummaryDetails

Associated Components