Sketch curve gets deleted when trying to trim it

2024-05-07T02:04:48Z

Summary


Details

After creating a sketch curve in a drawing view, when attempting to trim it with a hidden line shape, the sketch curve is deleted.

Reproduced Steps:

1. Prepare a model ( a box solid) and a drawing view


2. Create a sketch curve > Trim command > select the sketch curve as Curve to Trim

Before selecting:


After selecting:


Solution

This behavior is working as expected.

The system searches for boundary curves among objects belonging to the same sketch. If no boundary curve exists, the sketch curve is completely deleted.

Workaround: Explicitly select boundary curves instead of automatically searching. (Select the boundary curves without first selecting the sketch curve to trim.)

Notes

This behavior is the same in 3D modeling environment.

**Please refer to PL8789975 for Japanese article.

Release Versions
  • NX V2312
  • NX - DRAFTING V2312
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8789977

Contents

SummaryDetails

Associated Components