Expression control for "Assign Feature Color"

2024-05-17T02:41:43Z

Summary


Details

Changing feature colors requires executing the command each time, which is very time-consuming. Is it possible to control the color using an expression during or after command execution?

Reproduced Steps:

Home tab > Base group > More > Assign Feature Color > Feature Face Color > Specify Color > choose a color from the Object Color Palette > select a feature > OK


Solution

It cannot be controlled by the expressions. Please perform the command and change the color each time.

Workaround: This can be achieved with the “Color Expression” command.

After Mold environment > Menu > Tools > Mold and Die > Mold Wizard > Mold Tools > Color Expression...


Notes

"Color Expression" command requires Mold Wizard or Progressive Die Wizard license.

This command uses the "ug_mold_design" license feature. Even if you do not have a license, you can use it with 63 tokens.

**Please refer to PL8789968 for Japanese article.

Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8789971

Contents

SummaryDetails

Associated Components