Solid Edge 2024 Update 5 Announcement

2024-04-29T13:02:26Z

Summary


Details

April 29, 2024

Dear Solid Edge Customer:

Solid Edge 2024 Update 5 is now available for download.

We appreciate your continued business and participation in the software support process. Your feedback helps us improve Solid Edge and better serve your business needs.

Sincerely,

The Solid Edge Team

============

Release Notes:

============

Solid Edge 2024 Update 5

Version: 224.00.05.04

Download Solid Edge 2024 (2310) Updates

If clicking the direct download URL does not resolve in your browser, please go ahead, and navigate from the top-level Support Center.

===============

Email Notification:

===============

To receive direct email notifications for Solid Edge Updates, navigate to your Support Center Profile (https://account.sw.siemens.com/profile, scroll to Newsletter Subscriptions, and check the box for Software Field Bulletin

==========================================

This Solid Edge Update resolves the following PRs:

==========================================

===Assembly===

PR 11033751: The Cut Length in the Bend Table is incorrect.

PR 10855876: Delay when opening an assembly.

PR 10976192: 3D Sketch broken when the fitting is not found with Piping Route.

PR 11024916: Issues with RCS point cloud origin.

PR 12014061: The “Dim surrounding components when a selection is made in relationship pathfinder” option is not working.

PR 10600509: Manual weldment feature does not carry over with STP conversion.

PR 10914478: PathFinder content disappears while expanding a selected subassembly.

PR 12018219: Editing a Pattern feature causes constraints and other features to fail.

PR 10968633: Components are hidden in higher level.

PR 11025475: XpresRoute Tube Flat Length incorrect.

PR 11036374: Crash when opening material table in assembly for part w custom property.

PR 11045099: Adjustable assemblies not updating changes in base assembly/part.

PR 11045516: Explode flowlines do not update graphically.

PR 9515056: Users are inundated with Favorite/Recent Material(s) errors when opening an assembly.

===Draft===

PR 11007194: When a drawing view is placed, a second view is placed at the origin.

PR 11029060: Solid Edge closes when creating PMI view.

PR 11019544: Section fill style not pulling correctly on the internal parts.

===General===

PR 11015586: Cloud Gateway - Sign In fails with: String was not recognized as a valid Date Time.

PR 11008283: Solid Edge hangs when going to Discovery Center.

===Part/Profile/Sheetmetal===

PR 10914391: Variables are duplicated.

PR 11041605: Crash when opening Hole Options.

PR 11004084: Changing Round-off in SmartDim Feature Callout results in code displayed.

===SEEC===

PR 10946369: Solid Edge crashed during replace part with copy and edit in place command.

PR 10936268: The parent of FOA does not get updated unless we close the saved FOA opened using the Edit->Open command.

PR 10987838: Solid Edge showing new version of Assembly.

PR 12015793: Opening from RAC checks out the file but remains read-only in Solid Edge.

PR 12006908: During revision a PDF is generated that has 2 named references.

PR 12014337: Using multiple revisions of documents with "Hide" option.

===Solid Edge Data Management===

PR 11047313: Reproducible Solid Edge crash when modify Options > Solid Edge Data Management.

PR 10971748: Rename and Copy does not work.

PR 10979375: Where used Folder dialog should not show up at multi file check.

PR 10993474: Specified Revision number property content will be removed in Design Manager.

PR 11023033: Design Manager-Rename clear Revision Number Field.

===TechPub===

PR 11030153: Insistent range of html file sizes.

===Translators===

PR 11027391: Cannot open Inventor 2024 ipt in Solid Edge 2024.

PR 11003098: Unable to create a JT file from assembly.

KB Article ID# PL8789378

Contents

SummaryDetails

Associated Components