Solid Edge Editing part is painfully slow.

2024-05-07T18:49:08Z
ASSEMBLY

Summary


Details

Slow performance in Sketch in in-place edited part in a complex assembly.

Platforms
  • INTEL windows-1064
Release Versions
  • Solid Edge V224.0
Solution

This can be caused by the computer being overwhelmed by the amount of data Solid Edge is trying to locate in the rest of the assembly. Turning off Peer Edge Locate and Component Locate will reduce this and return Solid Edge performance to a more acceptable level.

Notes

KB Article ID# PL8789051

Contents

SummaryDetails

Associated Components

ASSEMBLY: ANNOTATIONS/DIMENSIONS