AW Gap/DPV: Unexpected options to add a DPV Excel workbook in AW
SPMEOPR
Go to AWS
Click on DPV icon
Perform a search on BCF16860
Highlight the DPV Inspection
Click Attachments
Click Add to under Files
Hit Type
Go down to items beginning with 'DPV'
*** Need clarification on selection for DPV workbook.
Need clarification on selection for DPV workbook. See attachments for AW options and file types on existing workbooks.
The following Display rules are present on the objects in BMIDE, and can be seen in the .syslog:
<TcTypeDisplayRule hiddenTypeName="DPVExcel" accessorName="Organization" accessorType="Organization"
conditionName="isTrue" description=""/>
<TcTypeDisplayRule hiddenTypeName="DPVRDL" accessorName="Organization" accessorType="Organization"
conditionName="isTrue" description=""/>
Display rules are preventing the DPV dataset types from displaying as options
Necessary BMIDE change was made to demonstrate that EWB can now be uploaded via Active Workspace.
Notes