Unable to use the Select Similar Faces function

2024-04-29T11:50:12Z

Summary


Details

When the user tries to use the Select Similar Faces function, NX returns an error about a missing license:

License Error, The check out of a feature failed because its token feature does not exist.


Solution

Recent versions of NX have added some powerful smart selection tools for manufacturing.  These new selection functions do require additional licenses:

- nx_ml_region_finder 

When "Select Similar Faces" command is used, "nx_ml_region_finder" is consumed. Menu > Edit > Selection > Select Similar Faces This command available on NX 2206 and later.

- nx_ml_sel_pred_std 

If "nx_ml_sel_pred_std" is available, When selecting an object "Selection Prediction Options" appears in Scene Bar. For example; When an edge is selected with Edge Blend command. If "nx_ml_sel_pred_std" is unavailable, "Selection Prediction Options" does not appear in Scene Bar.

- nx_ml_show_hide 

When "Select Similar Components" command is used, "nx_ml_show_hide" is consumed. Menu > Edit > Selection > Select Similar Components

In this case, if the license feature "nx_ml_region_finder" is not listed in your license, you cannot use the "Select Similar Face" functionality.  Please contact your Siemens sales representative for information on adding this to the site license file.  

Notes

See also NX2312 help page on Select Similar Faces:

https://docs.sw.siemens.com/en-US/doc/209349590/PL20230425446868577.selecting_objects/xid2210693

KB Article ID# PL8787138

Contents

SummaryDetails

Associated Components