April 23, 2024
Dear Solid Edge Customer:
Solid Edge 2023 Update 12 is now available for download.
We appreciate your continued business and participation in the software support process. Your feedback helps us improve Solid Edge to serve your business needs better.
Sincerely,
The Solid Edge Team
============
Release Notes:
============
Solid Edge 2023 Update 12
Version: 2210.0012.003 x64
Download Solid Edge 2023 (2210) Updates
Note: if the direct download URL doesn't resolve in your browser, please navigate from the top-level Support Center.
===============
Email Notification:
===============
To receive direct email notifications for Solid Edge Updates, navigate to your Support Center Profile (https://account.sw.siemens.com/profile, scroll to Newsletter Subscriptions, and check the box for Software Field Bulletin.
==========================================
This Solid Edge Update resolves the following PRs:
==========================================
===Assembly===
PR 10946369: Solid Edge crashed during a replace part with copy and edit in place command.
PR 10976192: 3D Sketch broken when the fitting is not found with Piping Route.
PR 10855876: Delay when opening an assembly.
PR 10893167: The drawing does not update due to assembly features not automatically recomputing.
PR 12012546: File open performance due to a large number of Thread Styles
PR 10600509: Manual weldment feature renaming does not carry over with STP conversion.
PR 10878110: A subassembly part does not show up graphically at a higher level.
PR 10914478: PathFinder content disappears while expanding a selected subassembly if 'Auto-scroll Assembly Pathfinder is ON.
PR 10968633: Components are hidden at higher level.
PR 11036374: Crash when opening the material table in assembly for a part with custom properties.
PR 11045099: The adjustable tube at the higher-level assembly does not reflect changes made to the original tube.
PR 12018219: Editing a Pattern feature causes constraints and other features to fail.
===Draft===
PR 11029060: Solid Edge closes when creating a PMI view.
PR 12013212: Customer is experiencing random crashes in Draft.
===Part/Profile/Sheetmetal===
PR 10914391: Variables are duplicated in the variable table after modifying a variable.
PR 10880296: Solid Edge crashes when opening the drop-down of Use Gage Table and pressing Win+shift+s'.
PR 10907910: The accept button is hidden behind the pull-down menu in the Break Corner.
===SEEC===
PR 10936268: The parent of FOA does not get updated unless we close the saved FOA opened using.
PR 10853494: AWC duplicate functionality reset to ItemID values for all the Item/revision names.
PR 10896801: Many crashes with Solid Edge after upgrading to Solid Edge 2023.
PR 10987838: Solid Edge is showing a new version of Assembly.
PR 12015793: Opening from RAC checks out the file but remains read-only in Solid Edge.
PR 12006908: A PDF with 2 named references is generated during revision.