How to Reset Existing Dimensions to a Drafting Standard.
Solution1. In Drafting, in the Top Border Bar, set the Type Filter to Dimension.
2. Select all the dimensions that need to be reset.
- Note: To select all dimensions, in the Top Border Bar choose Select All or Ctrl+A.
3. Right click a highlighted dimension and select Settings.
4. In the Settings dialog, under the Inherit group, change Settings Source to Customer Defaults.
5. Click Load from Settings Source.
6. Click Close.
- Note: This can be done to other drafting entities, such as Notes or Symbols and will reflect the drafting standard as set in Customer Defaults.