VRC Servers update for KUKA_REAL_TIME

2024-04-18T04:49:09Z

Summary


Details

Dear Siemens Digital Industries Software Customer,

We are pleased to inform you that VRC Servers for "KUKA_REAL_TIME"

are available for download from https://support.sw.siemens.com.

See <VrcServerName>_changes_log.htm for details

Note: This file is located in the 'Process Simulate VRC Servers Change Logs' folder directly under the 'Process Simulate VRC Servers' folder.

Use the following steps to download:

- Login to https://support.sw.siemens.com

- If you do not have an account, click 'Register Now' and fill out the information.

- Once on Support Center, if you do not see Tecnomatix under 'My Products', click 'Manage Products'.

- Scroll down and toggle On the Tecnomatix product.

- Scroll back to the top and click Support Center in the breadcrumb.

- Select 'Tecnomatix' from 'My Products'

- Select 'Download'

- Select 'Additional Downloads'

- Select 'Process Simulate VRC Servers'

- Select KUKA_REAL_TIME

Download the file(s):

TECNOMATIX_VRC_SERVER_KUKA_REAL_TIME_v1.2.2_17_04_2024.exe

To Install:

Place <VrcServerName>_<Version>_<Date>.exe into a folder ($VRC/downloads is suggested, where $VRC is the full path to the VRC Software installation).

Run <VrcServerName>_<Version>_<Date>.exe.

The default installation point is C:\Program Files

Notes: For the UNIVERSAL VRC Server, the debian distribution should be installed in the URSIM Virtual Machine, as follows:

sudo dpkg -i TECNOMATIX_VRC_SERVER_UNIVERSAL_REAL_TIME_<Version>_<Date>.deb

For the ABB VRC MANAGER, the zip file should be decompressed and the VRC Manager.msi should be executed.

If you have any issues with the installation or support of these fixes,

please contact your local GTAC support group.

Sincerely,

Siemens Digital Industries Software

KB Article ID# PL8787083

Contents

SummaryDetails

Associated Components