Report Only "Inspection Dimension" in Solid Edge Inspector

2024-04-19T13:10:52Z

Summary


Details

A user needs that only Inspection Dimensions be outputted into a Solid Edge Inspector Report.

Is it possible to create a Characteristic Number (CN) list and do a Report with Solid Edge Inspector that shows only selected dimensions?

When the user selects some dimensions and specifies them as "Inspection Dimension"...


...then creates via the Ballooning command the CN List, all dimensions (Inspection dimensions and Default dimensions) will be processed.


Doing a Report, all dimensions are listed - not only the Inspection Dimensions: 



Solution

The workaround is to create a CN by selection to apply only characteristic numbers of certain dimensions.  

Open the draft and select only the dimensions which need to be set as Inspection Dimensions.


Then select the CN command from Solid Edge Inspector menu and select again the dimensions to process:


Once the CN list has been created - only for the selected dimensions - select the Report command:


The Report will correctly show only the specified Inspection Dimensions.


KB Article ID# PL8786672

Contents

SummaryDetails

Associated Components