Solid Edge Inspector Error When Creating a CN List

2024-04-19T12:50:18Z

Summary


Details

In the Solid Edge draft environment, when the user tries to apply Ballooning and create a new CN (Characteristic Number) list the following Solid Edge Inspector error occurs:



Solution

This happens when the General Tolerances Table is not defined.

To solve this problem you need to select the "General Tolerances" command from Solid Edge Inspector menu:


and select from "Description" one of the Defined Tolerance Tables:



Then the Ballooning operation will be correctly executed:


KB Article ID# PL8786655

Contents

SummaryDetails

Associated Components