Combine Rotary - Unwanted Rotary Move at Equator Positions

2024-04-15T13:48:49Z

Summary


Details

Extra Rotary Output when the Postbuilder is using the imported tcl custom command. pb_cmd_combine_rotary.tcl

Solution
#--------------------------------------------------------------------------- # Set this flag to also output rotary angles at equator (0, +/-180, +/-360) # => Comment out next line or set it to "0" to suppress the output - set ::mom_sys_combine_rotary_output_equator_angles 1

Place a "#" sign in front of the following line when you don't want the equator values output. See below...

# set ::mom_sys_combine_rotary_output_equator_angles 1

                                                       or

set ::mom_sys_combine_rotary_output_equator_angles 0

KB Article ID# PL8786593

Contents

SummaryDetails

Associated Components