Colour Blindness settings in NX

2024-04-12T05:06:36Z

Summary


Details

How to help colorblind users adjust the color palette

Solution

In older NX Versions the Variable UGII_OVERRIDE_CDF was used as a “Undocumented Variable” . This has been removed, there is a better solution and more efficient solution for colorblind person.

Please use the following:

Start from Windows 10 /11, NX both graphics display and menu toolbar display can benefits from operation system provided better functionality through.

WIN 10:

"Start > Settings > Ease of Access > Color filters" and turn on "Turn on color filters".  

WIN11:

"Start > Settings > Accessibility > Color filters" Turn on color filters / Keyboard Shortcuts.  


An advantage of this method is that this setting is just as helpful with all windows applications as it is with NX.

Reference Link:

Use color filters in Windows - Microsoft Support

https://support.microsoft.com/en-us/windows/use-color-filters-in-windows-43893e44-b8b3-2e27-1a29-b0c15ef0e5ce#:~:text=to%20Color%20filters-,To%20use%20a%20color%20filter%3A,Ease%20of%20Access%20%3E%20Color%20filters.

Notes

KB Article ID# PL8786404

Contents

SummaryDetails

Associated Components