Keyshot - Full Animation Module Needed

2024-04-30T16:38:30Z

Summary


Details

In this example, the user follows this workflow:

Create an animation in 'Solid Edge ERA/Animation Editor'.

Then selects 'Keyshot animate'.

Keyshot 11 opens.

Select 'animation' and 'animation wizard'.

Then the "Note: Upgrade to the full Animation module to enable all animation features" shows.

How to solve this issue?

Platforms
  • na windows-1064
Release Versions
  • Solid Edge V224.0
Solution

This issue is resolved in the KeyShot 2024.1 version that will be delivered with Solid Edge 2025.

However, you can also download KeyShot 2024.1 from Luxion:

https://www.keyshot.com/resources/downloads/?gate=download&submissionGuid=0dba9613-1a31-42df-a8b7-4430e8cf1409

Then you will be able to run the animation from Solid Edge ERA inside of Keyshot.

Notes

KB Article ID# PL8786272

Contents

SummaryDetails

Associated Components