After TDP export, datum is displayed in Acrobat Reader

2024-04-09T23:18:57Z

Summary


Details

When exporting TDP, the datum of each components is also exported. Is there any setting that doesn't export it?

Reproduced Steps:

1. PMI tab > Publish > 3D PDF


2. Open the exported PDF in PDF Reader such as Acrobat Reader


Solution

When exporting TDP, there is no setting to control the output of the datum coordinate system.

Workaround: Controlled on PDF reader side such as Acrobat Reader. Or hide/delete it in NX before exporting TDP.

Below example, DATUM_CSYS is turned off in the model tree.


Notes

**Please refer to PL8785794 for Japanese article.

Release Versions
  • NX V2206
  • NX - TECH_DATA_PKG V2206
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8785796

Contents

SummaryDetails

Associated Components