Where to obtain the Solid Edge COMPOSITE2 Host ID number ?

2024-04-09T14:09:23Z

Summary


Details

When activating a Node Locked Solid Edge License, you need to provide the COMPOSITE2 Host ID number (CID2) for the machine.  Where can that be obtained?

Solution

There are two ways to get this:

a) If you have already installed Solid Edge:

Click Start > Siemens Solid Edge License Utility.

Your CID2 is listed in the upper left in the Dialog Box:


Alternatively, you could go to the Program Folder of Solid Edge and open a Command prompt:

After that you enter:

getcid -composite2 

The result looks like this:


b) If you have not installed Solid Edge: 

This can be found in our Support Center Webpage.

Go to :  Downloads > Siemens License Server 

There you will find the SiemensLicenseServer_v2.4.0.0.hostid_utils.zip:


Download and unzip the file.  There you will find the getcid.exe which you can use in a Command Prompt.

Notes

If you have further inquiries about Node Locked Licensing please refer to the FAQs collection link below:

Solid Edge Node Locked License FAQs Collection

KB Article ID# PL8785511

Contents

SummaryDetails

Associated Components