When selecting PMI object output from TDP in Acrobat Reader, unrelated object is highlighted

2024-05-07T01:52:37Z

Summary


Details

When creating balloons or other PMIs, even though I have released the selected associated object, when I check it in Acrobat Reader after exporting to TDP, it's highlighted as associated object. Of course, selecting the PMI in NX does not highlight the object.

Reproduced Steps:

1. Prepare model data and create PMI such s Balloon( Release associated object once selected when creating PMI)


2. PMI tab > Publish > select the balloon in PDF Reader such as Acrobat Reader


Solution

This behavior is due to NX problem occurred in NX 2312 & lower, but it will be fixed in NX 2406 Series.

Workaround:

There is no workaround; avoid operations that create Leader line (Terminating Object) from the associated objects that are released.

Notes

The problem occurs with all PMI such as balloons, notes, and datums.

**Please refer to PL8785491 for Japanese article.

Release Versions
  • NX V2312
  • NX - TECH_DATA_PKG V2312.5000
Platforms
  • Windows x64 10
  • Windows x64 11

KB Article ID# PL8785491

Contents

SummaryDetails

Associated Components