Geometric Dimensioning and Tolerancing symbols are not correctly displayed

2024-04-04T08:09:24Z

Summary


Details

Geometric Dimensioning and Tolerancing (GD&T) symbols are not correctly displayed on the Solid Edge draft e.g.


Solution

This will occur when the Solid Edge fonts have not been installed onto the workstation e.g.

Start > Control Panel > Appearance and Personalisation > Fonts


The Solid Edge fonts can be downloaded and installed separately without having to uninstall and reinstall Solid Edge.

In Support Center locate the Solid Edge Add-ons download section for your Solid Edge version and download the Solid Edge fonts:


Open the downloaded Zip file and extract the content of the Fonts folder into a temp folder.

Select all the extracted fonts and right-click > Install for all users


If promoted that the font is already installed and do you want to replace it select Yes to replace all fonts


The Solid Edge fonts are now successfully installed


Restart Solid Edge and the missing GD&T symbols will now be correctly displayed


KB Article ID# PL8785300

Contents

SummaryDetails

Associated Components