Solid Edge Solid Edge 2021 (v221) End of Maintenance Information

2024-11-20T14:48:57Z
SETUP

Summary


Details

End of Standard Maintenance for Solid Edge 2021 (v221) suite of product is listed below. These dates represent when Siemens Digital Industries Software will discontinue providing ongoing maintenance releases and the last Teamcenter release supported. After these dates, no further maintenance releases will be issued for the corresponding Solid Edge version.    

Solution

Solid Edge Version End of Maintenance Dates  (Out of Maintenance)

2021 (v221) End of Maintenance (EoM):                    30th June 2022

Solid Edge & Teamcenter Integration

2021 (v221) MP1:                                                             Tc13.O, 13.1, 13.2, 13.3
2021 (v221) MP12:                                                           Tc14.1
2021 (v221) RTM:                                                             
Tc 11.3.0.1, 12.1, 12.2, 12.3,12.4, 12.5, 12.6
2021 (v221) RTM Standalone:                                       AW 3.4, AW 4.x, AW 5.x
2021 (v221) RTM Hosted:                                               AW 3.4, AW 4.x, AW 5.x
2021 (v221) RTM:                                                             Geolus 9 AW 4.1.2, Geolus 10 AW 4.3

Click here and follow the information to review the detailed, actual "End of Maintenance dates for Teamcenter Integrations" (Solid Edge & Teamcenter Integration EoM SFB v301024.pdf) Information.

Notes

You are looking for another Solid Edge Version End of Maintenance Information? Go to Solid Edge and Solid Edge X Version End of Maintenance Information (Collection)

Support Information

PLMS will continue to provide support and assistance for Solid Edge. PLMS will attempt to duplicate any possible code defects on the revision of software the defect is reported (when available) and on the current release or Update of the product. PLMS will not write a PR unless the problem can be duplicated in a supported version of the product. If it is found that the defect does not occur in the latest revision of the software, the customer will be asked to update their product to the current revision to correct the problem.  

KB Article ID# PL8785185

Contents

SummaryDetails

Associated Components

SETUP: INSTALL SETUP: LICENSING