Solid Edge 2023 (v2210) End of Maintenance Information

2024-11-20T14:48:41Z

Summary


Details

End of Standard Maintenance for Solid Edge 2023 (v2210) suite of products is listed below. These dates represent when Siemens Digital Industries Software will discontinue providing ongoing Maintenance releases along with the last Teamcenter release supported.  After these dates, no further maintenance releases will be issued for the corresponding Solid Edge version.

Solution

Solid Edge Version End of Maintenance Dates               (Out of Maintenance) 

2023 (v2210) End of Maintenance (EoM):                          31st July 2024

Solid Edge & Teamcenter Integration

2023 (v2210) 11:                                                                      Tc15 (Tc2312)
2023 (v2210) RTM:                                                                  Tc12.0 Limited
2023 (v2210) RTM:                                                                  
Tc13.0, Tc14.0
2023 (v2210) RTM:                                                                  Geolus 2206 Tc14.x, Tc13.x

Click here and follow the information to review the detailed, actual "End of Maintenance dates for Teamcenter Integrations" (Solid Edge & Teamcenter Integration EoM SFB v301024.pdf) Information.

Notes

If you are looking for another Solid Edge Version End of Maintenance Information go to Solid Edge and Solid Edge X Version End of Maintenance Information (Collection)

Support Information

PLMS will continue to provide support and assistance for Solid Edge.  PLMS will attempt to duplicate any possible code defects in the revision of software in which the defect is reported (when available) and on the current release or Update of the product.  PLMS will not create a PR unless the problem can be duplicated in a supported version of the product.  If it is found that the defect does not occur in the latest revision of the software, the customer will be asked to update their product to the current revision to correct the problem.

KB Article ID# PL8785104

Contents

SummaryDetails

Associated Components