Customer Default to Control the Gap Setting in Centerlines

2024-04-08T11:33:08Z

Summary


Details

 How to set the Customer Defaults for Gap Settings in 2D, 3D, and Symmetrical Centerline, Circular Centerline, Bolt Circle Centerline and Center Mark.

Solution

 1. Select File-> Utilities-> Customer Defaults.

2. Under Drafting-> General/Setup, on the Standards tab, select a default standard to Customize


3. Configure the Gap settings as needed

4. Save  and restart NX.

5. Now when a  centerline/mark or any of the below are created, they will all have the settings configured in the Drafting Standard set in Customer Defaults.


 The gap settings for all the centerlines/marks are controlled by the same  Drafting Standard set in the Customer Defaults.

KB Article ID# PL8784943

Contents

SummaryDetails

Associated Components