getcid returns "no Siemens Software Licensing Composite HostID"

2024-07-30T17:12:56Z

Summary


Details

When running getcid.,exe, it returns "There is no Siemens Software Licensing Composite HostID for this host "XXXXXXXX" e,g,


Solution

This no "Composite HostID" message can occur if the "Internet Protocol Version 4 (TCP/IPv4)" is not enabled on the physical network adapter.

Simply enable IPv4 on the physical network adapter using the following steps...

Start > Control Panel > Network and Internet > Network and Sharing Centre > Change adapter settings:


Select the physical network adapter and right-click > Properties


In the Networking tab select and check on the "Internet Protocol Version 4 (TCP/IPv4)" option:


Select OK to accept the changes.

Run getcid.exe again and this time a valid Composite HostID will be returned:


Notes

If you have further inquiries about Solid Edge Floating Licensing please refer to the FAQs collection link below:

Solid Edge Floating License FAQs Collection

KB Article ID# PL8784934

Contents

SummaryDetails

Associated Components